ROBOTIS e-Manual v1.29.00

AX Series

Connection to UART  

To control the Dynamixel actuators, the main controller needs to convert its UART signals to the half duplex type. The recommended circuit diagram for this is shown below.

  
 

Pin Assignment

The connector pin assignments are as the following. The two connectors on the Dynamixel are connected pin to pin, thus the AX-12 can be operated with only one connector attached.

  
 

Confirmation of Connection

The LED of AX-12 flickers once if the power is supplied to AX-12 properly via wiring.

 



Error Report

Copyrights (c) 2010  ROBOTIS  All rights reserved.