MX-106T / MX-106R

Parts Photo

  

[MX-106T]                                   [MX-106R]

 

 

※ Control Table’s Compliance replaced by PID.

The control tables order for PID has changed to DIP from this version onwards. Please make reference of this change.

Although the MX-106T (TTL) and MX-106R (RS-485) differ in communications protocols both have the same features and perform equally. (TTL uses 3-pin connectors while RS-485 uses 4)

In order to use Protocol 2.0, please update the firmware to V39 or above. (Update firmware using R+ Manager 2.0, Youtube)

For MX-106 (2.0) Protocol, please refer to the MX-106 (2.0) Control table as they are different.

 

H/W Specification

 

Stall torque : Peak stall torque read from transient state  

Performance graph (N-T Curve) : A graph shows torque measured in stable condition while increasing load

*Normally, stall torque is bigger than maximum torque on performance graph.

 

Precautions when connecting to power supply!

- For the stable power supply, we recommend using ROBOTIS controller or SMPS2Dynamixel.

- Connect your DYNAMIXEL to power supply while it’s off and turn on/off with the power switch.

 

Control Table

Control Table consists of data regarding the current status and operation, which exists inside of Dynamixel. The user can control Dynamixel by changing data of Control Table via Instruction Packet.

EEPROM and RAM

Data in RAM area is reset to the initial value whenever the power is turned on while data in EEPROM area is kept once the value is set even if the power is turned off.

Note : Two's complement rule is followed to find the negative value in multi turn mode.

For more information, please refer to the following link (Two's complement link).

Address

It represents the location of data. To read from or write data to Control Table, the user should assign the correct address in the Instruction Packet.

Access

Dynamixel has two kinds of data: Read-only data, which is mainly used for sensing, and Read-and-Write data, which is used for driving.

Initial Value

In case of data in the EEPROM Area, the initial values on the right side of the below Control Table are the factory default settings. In case of data in the RAM Area, the initial values on the right side of the above Control Tables are the ones when the power is turned on.

Highest/Lowest Byte

In the Control table, some data share the same name, but they are attached with (L) or (H) at the end of each name to distinguish the address. This data requires 16bit, but it is divided into 8bit each for the addresses (low) and (high). These two addresses should be written with one Instruction Packet at the same time.

 

Area

Address (Hexadecimal)

Name

Description

Access

Initial Value

(Hexadecimal)

E

E

P

R

O

M

0 (0X00)

Model Number(L)

Lowest byte of model number

R

64 (0X40)

1 (0X01)

Model Number(H)

Highest byte of model number

R

1 (0X01)

2 (0X02)

Version of Firmware

Information on the version of firmware

R

-

3 (0X03)

ID

ID of Dynamixel

RW

1 (0X01)

4 (0X04)

Baud Rate

Baud Rate of Dynamixel

RW

34 (0X22)

5 (0X05)

Return Delay Time

Return Delay Time

RW

250 (0XFA)

6 (0X06)

CW Angle Limit(L)

Lowest byte of clockwise Angle Limit

RW

0 (0X00)

7 (0X07)

CW Angle Limit(H)

Highest byte of clockwise Angle Limit

RW

0 (0X00)

8 (0X08)

CCW Angle Limit(L)

Lowest byte of counterclockwise Angle Limit

RW

255 (0XFF)

9 (0X09)

CCW Angle Limit(H)

Highest byte of counterclockwise Angle Limit

RW

15 (0X0F)

10 (0X0A)

Drive Mode

Dual Mode Setting

RW

0(0X00)

11 (0X0B)

the Highest Limit Temperature

Internal Limit Temperature

 RW

80 (0X50)

12 (0X0C)

the Lowest Limit Voltage

Lowest Limit Voltage

RW

60 (0X3C)

13 (0X0D)

the Highest Limit Voltage

Highest Limit Voltage

RW

160 (0XA0)

14 (0X0E)

Max Torque(L)

Lowest byte of Max. Torque

RW

255 (0XFF)

15 (0X0F)

Max Torque(H)

Highest byte of Max. Torque

RW

3 (0X03)

16 (0X10)

Status Return Level

Status Return Level

RW

2 (0X02)

17 (0X11)

Alarm LED

LED for Alarm

RW

36 (0X24)

18 (0X12)

Alarm Shutdown

Shutdown for Alarm

RW

36 (0X24)

20 (0X14)

Multi Turn Offset(L)

multi-turn offset least significant byte (LSB)

RW

0 (0X00)

21 (0X15)

Multi Turn Offset(H)

multi-turn offset most significant byte (MSB)

RW

0 (0X00)

22 (0X16)

Resolution Divider

Resolution divider

RW

1 (0X01)

R

A

M

24 (0X18)

Torque Enable

Torque On/Off

RW

0 (0X00)

25 (0X19)

LED

LED On/Off

RW

0 (0X00)

26 (0X1A)

D Gain

Derivative Gain

RW

0 (0X00)

27 (0X1B)

I Gain

Integral Gain

RW

0 (0X00)

28 (0X1C)

P Gain

Proportional Gain

RW

32 (0X20)

30 (0X1E)

Goal Position(L)

Lowest byte of Goal Position

RW

-

31 (0X1F)

Goal Position(H)

Highest byte of Goal Position

RW

-

32 (0X20)

Moving Speed(L)

Lowest byte of Moving Speed (Moving Velocity)

RW

-

33 (0X21)

Moving Speed(H)

Highest byte of Moving Speed (Moving Velocity)

RW

-

34 (0X22)

Torque Limit(L)

Lowest byte of Torque Limit (Goal Torque)

RW

ADD14

35 (0X23)

Torque Limit(H)

Highest byte of Torque Limit (Goal Torque)

RW

ADD15

36 (0X24)

Present Position(L)

Lowest byte of Current Position (Present Velocity)

R

-

37 (0X25)

Present Position(H)

Highest byte of Current Position (Present Velocity)

R

-

38 (0X26)

Present Speed(L)

Lowest byte of Current Speed

R

-

39 (0X27)

Present Speed(H)

Highest byte of Current Speed

R

-

40 (0X28)

Present Load(L)

Lowest byte of Current Load

R

-

41 (0X29)

Present Load(H)

Highest byte of Current Load

R

-

42 (0X2A)

Present Voltage

Current Voltage

R

-

43 (0X2B)

Present Temperature

Current Temperature

R

-

44 (0X2C)

Registered

Means if Instruction is registered

R

0 (0X00)

46 (0X2E)

Moving

Means if there is any movement

R

0 (0X00)

47 (0X2F)

Lock

Locking EEPROM

RW

0 (0X00)

48 (0X30)

Punch(L)

Lowest byte of Punch

RW

0 (0X00)

49 (0X31)

Punch(H)

Highest byte of Punch

RW

0 (0X00)

68 (0X44)

Current(L)

Lowest byte of Consuming Current

RW

0 (0X00)

69 (0X45)

Current(H)

Highest byte of Consuming Current

RW

0 (0X00)

70 (0X46)

Torque Control Mode Enable

Torque control mode on/off

RW

0 (0X00)

71 (0X47)

Goal Torque(L)

Lowest byte of goal torque value

RW

0 (0X00)

72 (0X48)

Goal Torque(H)

Highest byte of goal torque value

RW

0 (0X00)

73 (0X49)

Goal Acceleration

Goal Acceleration

RW

0 (0X00)

 

 

Address Function Help

EEPROM Area

Model Number

It represents the Model Number.

 

Firmware Version

It represents the firmware version.

 

ID

It is a unique number to identify Dynamixel.

The range from 0 to 252 (0xFC) can be used, and, especially, 254(0xFE) is used as the Broadcast ID.
If the Broadcast ID is used to transmit Instruction Packet, we can command to all Dynamixels.

 

Please be cautious not to have the same IDs for the connected dynamixels. You may face communication issues or may not be able to search when IDs overlap.

 

Baud Rate

It is the baud rate to communicate with controller. It is available in between 0~254(0XFE).

 

If the data value is in between 0~249 :

Baudrate(BPS)  = 2000000 / (Data + 1)

Data

Set BPS

Target BPS

Tolerance

1

1000000.0

1000000.0

  0.000 %

3

500000.0

500000.0

  0.000 %

4

400000.0

400000.0

  0.000 %

7

250000.0

250000.0

  0.000 %

9

200000.0

200000.0

  0.000 %

16

117647.1

115200.0

 -2.124 %

34

57142.9

57600.0

  0.794 %

103

19230.8

19200.0

 -0.160 %

207

9615.4

9600.0

 -0.160 %

 

If the date value is over the 250 :

Data

Set BPS

Target BPS

Tolerance

250

2250000.0

2250000.0

  0.000 %

251

2500000.0

2500000.0

  0.000 %

252

3000000.0

3000000.0

  0.000 %

 

Note : Maximum Baud Rate error of 3% is within the tolerance of UART communication.

 

 

Return Delay Time

It is the delay time per data value that takes from the transmission of Instruction Packet until the return of Status Packet.

0 to 254 (0xFE) can be used, and the delay time per data value is 2 usec.

That is to say, if the data value is 10, 20 usec is delayed. The initial value is 250 (0xFA) (i.e., 0.5 msec).

 

CW/CCW Angle Limit

Sets allowable position values (angles) for Goal Position (address 30 & 31)  

• CW Angle Limit: Goal Position(Address 30, 31) minimum value

• CCW Angle Limit: Goal Position(Address 30, 31) maximum value

The following sets 2 modes operation based on CW and CCW values

Operation Type

CW / CCW

Wheel Mode

 both are 0

Joint Mode

neither at 0

Multi-turn Mode

both are 4095

Wheel mode allows the motor can have limitless revolutions.

Joint mode allows robot with multiple joints

Multi-turn mode allows joints have range of controllable position values from -28672 to 28672.

 

Multi Turn Offset

Adjusts position (zeroing). This value gets included in Present Position (36).

Present position + multi-turn offset.

Initial value is 0 and range is from -24576 to 24576

A Dynamixel with a position of 2048 with an applied offset of 1024 outputs a Present position of 3072.

  

Note: This feature is only applied in multi-turn mode and ignored in other modes.

 

Resolution Divider

It allows the user to change Dynamixel’s resolution.

The default Resolution Divider Value is set as 1. (1 ~ 4 available)

When resolution is lowered, revolutions (in both directions) can be increased (up to 28 turns in each direction).

Present Position = Real Position / Resolution Divider

For example, a Real Position of 2048 with a Resolution Divider set as 2 will yield a Present Position value of 1024 (2048/2 = 1024). A Dynamixel with Resolution Divider set as 2 will have a resolution 2048 for a single revolution.

The Present Position can be obtained while Multi-turn Offset and Resolution Divider are taken into account.

Present position = (Real Position / Resolution Divider) + Multi-turn Offset

For example, a Dynamixel with a Real Position of 2048 with a Resolution Divider set as 4 and Multi-turn Offset as 1024 will yield a Present Position of 1535 ((2048/4) + 1024 = 1535).

Note: This feature is only applied in multi-turn mode and ignored in other modes.

 

Drive Mode

Drive mode is set for Dynamixel.

 

Bit

Name

Contents

Bit 7

N/A

-

Bit 6

N/A

-

Bit 5

N/A

-

Bit 4

N/A

-

Bit 3

N/A

-

Bit 2

N/A

-

Bit 1

Master/Slave Mode

In case of 0: Master mode, In case of 1 : Slave mode

Bit 0

Normal/Reverse Mode

In case of 0: Normal mode, In case of 1: Reverse mode

Notes : Reverse mode is to change the actual rotation direction reversely.  It can be used conveniently when the robot with symmetrical joints layout is built.

 

Dual Joints

Dual joints are used as 1 joint by controlling 2 motors simultaneously.  

To use the dual joints, 1 unit of motor set in master mode and 1 unit of motor set in slave mode are needed.

Next, the motors must be connected to each other using synchronization cable.

 

Normal mode synch cable: Drives Master and PWM signals synchronized

Reverse mode synch cable: Drives PWM signals in reverse.

 

Notes : Slave is synchronized by directly receiving the control command through synchronization cable from Master.  Slave Mode unit responds to communication through command packets, but data related to motor drive are processed only through the synchronization.

 

For reference: in a dual master-slave configuration position information from the slave is ignored and the position of the dual configuration is based on the master in PWM control.

When master and slave are not physically connected the is a slight difference on the driven load.

Use the frames shown below to achieve dual configuration

 

The Highest Limit Temperature

Caution : Do not set the temperature lower/higher than the default value.

When the temperature alarm shutdown occurs, wait 20 minutes to cool the temperature before re-use.

Using the product when the temperature is high may and can cause damage.

 

The Lowest (Highest) Limit Voltage

It is the operation range of voltage.

50 to 160 (0x32 ~ 0xA0) can be used.  The unit is 0.1V.

For example, if the value is 80, it is 8V.

If Present Voltage (Address42) is out of the range, Voltage Range Error Bit (Bit0) of Status Packet is returned as ‘1’ and Alarm is triggered as set in the addresses 17 and 18.

 

Max Torque

It is the torque value of maximum output. 0 to 1023 (0x3FF) can be used, and the unit is about 0.1%.

For example, Data 1023 (0x3FF) means that Dynamixel will use 100% of the maximum torque it can produce while Data 512 (0x200) means that Dynamixel will use 50% of the maximum torque. When the power is turned on, Torque Limit (Addresses 34 and 35) uses the value as the initial value.

 

Status Return Level

It decides how to return Status Packet. There are three ways like the below table.

Value

Return of Status Packet

0

  No return against all commands (Except PING Command)

1

  Return only for the READ command

2

  Return for all commands

 

When Instruction Packet is Broadcast ID, Status Packet is not returned regardless of Status Return Level.

 

Alarm LED

Alarm Shutdown

DYNAMIXEL can protect itself by detecting errors occur during the operation. The errors can be set are as the table below.


Bit

Name

Contents

Bit 7

0

-

Bit 6

Instruction Error

 When undefined Instruction is transmitted or the Action command is delivered without

  the reg_write command

Bit 5

Overload Error

 When the current load cannot be controlled with the set maximum torque

Bit 4

CheckSum Error

 When the Checksum of the transmitted Instruction Packet is invalid

Bit 3

Range Error

 When out-of-range value for target address is detected in the packet

Bit 2

Overheating Error

 When the internal temperature is out of the range of operating temperature set in

  the Control Table

Bit 1

Angle Limit Error

 When Goal Position is written with the value that is not between CW Angle Limit and CCW

  Angle Limit

Bit 0

Input Voltage Error

 When the applied voltage is out of the range of operating voltage set in the Control Table

It is possible to make duplicate set since the function of each bit is run by  the logic of ‘OR’.

That is, if 0X05 (binary 00000101) is set, both Input Voltage Error and Overheating Error can be detected.

When Alarm LED occurs, the LED blinks and when Alarm Shutdown occurs, the motor output becomes 0 % by making the value of Torque Limit (Address 34, 35) as 0.

     

RAM Area

Torque Enable

Value

Meaning

0

 Keeps Torque from generating by interrupting the power of motor.

1

 Generates Torque by impressing the power to the motor.

 

LED

Bit

Meaning

0

Turn OFF the LED

1

Turn ON the LED

 

PID Gain

MX series will use the PID controller as a main control method.

P gain refers to the value of proportional band.

I gain refers to the value of integral action.

D Gain refers to the value of derivative action.

Gains values are in between 0~254.

The relationship between Compliance Slop and PID

Slope

P Gain
8 128
16 64
32 32
64 16
128 8

The less the P gain, The larger the back lash, and the weaker the amount of output near goal position.

At some extent, it is like a combined concept of margine and slope.

It does not exactly match the previous concept of compliance. So it is obvious if you see the difference in terms of motion.

 

Explanation for PID required.

For the brief explanation about general PID, please refer to the website(link) below.

http://en.wikipedia.org/wiki/PID_controller

FYI, PID control theory is not only limited to the control of motor(actuator) but is a generic theory that can be applied to all kinds of control.

 

Goal Position

It is a position value of destination.

0 to 4095 (0xFFF) is available.  The unit is 0.088 degree.

If Goal Position is out of the range, Angle Limit Error Bit (Bit1) of Status Packet is returned as ‘1’ and Alarm is triggered as set in Alarm LED/Shutdown.

 

Moving Speed

 

Note: This mode allows to check max rpm. Any values set higher than max rpm will not take effect.

 

Torque Limit

It is the value of the maximum torque limit.  

0 to 1023 (0x3FF) is available, and the unit is about 0.1%.  

For example, if the value is 512, it is about 50%; that means only 50% of the maximum torque will be used.
If the power is turned on, the value of Max Torque (Address 14, 15) is used as the initial value.

 

Notes: If the function of Alarm Shutdown is triggered, the motor loses its torque because the value becomes 0.  At this moment, if the value is changed to the value other than 0, the motor can be used again.

 

Present Position

It is the current position value of Dynamixel.  

The range of the value is 0~4095 (0xFFF), and the unit is 0.088 degree.

In multi-turn mode range is from -28672 to 28672 with unit values dependent on Resolution Divider (0.088 * Resolution Divider)

 

Note: in multi-turn mode Present position depends on resolution divider and multi-turn offset For more information turn to the section on Multi Turn offset and Resolution Divider

 

Present Speed

Is the current moving speed.

0~2047 (0x000~0X7FF) can be used.

If a value is in the rage of 0~1023 then the motor rotates to the CCW direction.

If a value is in the rage of 1024~2047 then the motor rotates to the CW direction.

The 10th bit becomes the direction bit to control the direction; 0 and 1024 are equal.

The value unit is about 0.11rpm.

For example, if it is set to 300 then the motor is moving to the CCW direction at a rate of about 34.33rpm.

 

Present Load

It means currently applied load.

The range of the value is 0~2047, and the unit is about 0.1%.

If the value is 0~1023, it means the load works to the CCW direction.

If the value is 1024~2047, it means the load works to the CW direction.

That is, the 10th bit becomes the direction bit to control the direction, and 1024 is equal to 0.

For example, the value is 512, it means the load is detected in the direction of CCW about 50% of the maximum torque.

 

 

Notes: Present load is an inferred value based on the internal output value; not a measured value using torque sensor, etc. Therefore, it may be inaccurate for measuring weight or torque. It is recommended to use it for predicting the direction and size of the force being applied to the joint.

 

Present Voltage

It is the size of the current voltage supplied.

This value is 10 times larger than the actual voltage. For example, when 10V is supplied, the data value is 100 (0x64)

 

Present Temperature

It is the internal temperature of Dynamixel in Celsius.

Data value is identical to the actual temperature in Celsius. For example, if the data value is 85 (0x55), the current internal temperature is 85℃.

 

 

Registered Instruction

Value

Meaning

0

 There are no commands transmitted by REG_WRITE

1

 There are commands transmitted by REG_WRITE.

 

Notes: If ACTION command is executed, the value is changed into 0.

 

Moving

Value

Meaning

0

 Goal position command execution is completed.

1

 Goal position command execution is in progress.

 

Lock

Value

Meaning

0

 EEPROM area can be modified.

1

 EEPROM area cannot be modified.

 

Caution: If Lock is set to 1, the power must be turned off and then turned on again to change into 0.


Punch

Current to drive motor is at minimum.

Can choose vales from 0x00 to 0x3FF.

 

Current

Value at 2048(0x800) when current is consumption is idle.

Values higher than 2048(0x800) during positive current flow

Values lower than 2048(0x800) during negative current flow

The following is a method to calculate current flow

 

I = ( 4.5mA ) * (CURRENT 2048 ) in amps unit (A).

For example, 68 gives a value of 2148, which corresponds to 450mA of current flow.

 

 

Torque Control Mode Enable

Value

Meaning

0

Turn off the torque mode. Executes Joint mode or Wheel mode.

1

Turn on the torque mode. Cannot control the position or moving speed but only Torque.
When Torque Control Mode Enable is at 1, DYNAMIXEL behaves like the followings
1. DYNAMIXEL does not control the position or the moving speed.
2. DYNAMIXEL controls with goal torque value.
3. DYNAMIXEL does not react to whatever value in Goal position and Goal speed.
4. Because position/moving speed is not controller, DYNAMIXEL behaves as if it is in the wheel mode.

 

Goal Torque

These are the goal torque value

You can use 0 ~ 2047 (0x7FF), and the unit is 4.5mA.

(torque is directly proportional to the current value.)

If you use from 0~1023, torque is on toward CCW, and when you set it to 0, it stops.

If you use from 1024~2047, torque is on toward CW, and when you set it to 1024, it stops.

That means, 10th bit becomes the direction bit, which controls direction.

Goal Torque cannot be bigger than Torque Limit(34,35)

 

Goal Acceleration

This is Goal Acceleration value.

It can be used from 0~254(0XFE), and the unit is approximately 8.583 Degree / sec^2.

When it is set to 0, there is no control over acceleration and moves with the maximum acceleration of the motor.

When the goal speead is set to 0, there is no control over acceleration and moves with the maximum acceleration of the motor.

When it is set to 254, it becomes 2180 Degree / sec^2

For example, the current speed of Dynamixel is 0, and Goal acceleration is 10,

The speed of Dynamixel after 1 second will be 14.3 RPM.

 

 

Option Frame

The types of MX-106 option frame are as follows.

FR05-F101_FR08-X101

 

FR05-S101

 

FR08-B101

 

FR08-H101

 

FR08-H110_FR08-D101

 

 

Horn

The types of MX-106 Horn are as follows.

HN05-N102

 

HN05-I101

 

Ref: place careful attention when aligning the horn of the RX-64 to prevent misalignment.

Horn & Bearing Replacement

The horn is installed on the front wheel gear serration of the DYNAMIXEL whereas the bearing set is installed on the back.

Installing the Front Horn

Place the thrust horn washer into the actuator before inserting the horn

You must carefully align the horn to the wheel gear serration by aligning dots.

Once alignment is properly done, gently push the center of the horn toward the actuator.

Make sure that the horn washer is in place as you tighten the bolt.

Installing the Bearing Set

You may need to remove the bearing set from the previous actuator and reinstall it into the new actuator.

The bearing set can also be purchased separately.

As bearing set is rotating freely, therefore alignment is not required when assembling to DYNAMIXEL.

Combination

The following example shows the combination structure of option frames and horns.

 

 

 

 

Dimension

Drawing Information  :    MX-106Dimension.pdf

 

Frame Compatibility Guide(LINK)

 

Videos

HOW TO REPLACE GEARS