BT-410 Dongle(Master)

Part Photo

[ Picture : BT-410 Dongle]

 

Product Usage

BT-410 Dongle converts USB 2.0 interface and Bluetooth 4.0 Low Energy standard communication interface(Master).

If BT-410 Dongle is connected to the PC, it can be paired with a BT-410 Slave module to exchange data.

(Please refer to each product  page for instructions)

 

 

Example

Available Features with BT-410 Dongle and BT-410 Slave pair

 

Firmware Recovery

(Manager 2.0)

Firmware Update
(Manager 2.0)
Entry R+ Scratch Task 2.0
Download
Motion 2.0 Download
CM-50(PLAY700)

O

O

-

O

O

-

CM-150

O

O

-

-

O

-

CM-200

O

O

-

-

O

O

CM-530

O

O

-

-

O

O

OpenCM7.0

O

O

O

O

O

-

OpenCM9.04

O

O

-

-

O

O

Car Robot

-

-

O

O

-

-

 

Communication Mode

Utilizes a pairing mechanism that allows reliable 1:1 communication.

[1:1 Communication]

 

Checking Driver Installation

How to check whether the BT-410 Dongle driver is installed correctly is as follows.

  1. Connect BT-410 Dongle to the USB Port of PC.

     
  2. Select Manage in the popped-up menu shown by right-clicking My Computer.
     
  3. Check USB Serial Converter in Universal Serial Bus Controllers of Device Manager.

     
  4. Check USB Serial Port(COMx) in the list of Ports (COM & LPT).
    (COM Port number may vary depending on each system.)

 

Installing the Driver Manually

If you install the RoboPlus,  FTDI Driver (USB2Dynamixel, USB Downloader (LN-101) driver, BT-410 Dongle) is installed together automatically.
If you didn't install the RoboPlus yet, or if the driver is not installed appropriately, please install it manually according to following procedures.  

 

  1. Connect a device to PC. If the driver is not installed yet, Found New Hardware Wizard will be popped up.
    Install from a list or specific location (Advanced)(S) -> Next(N)
     
  2. Decide the location of Driver.
    If RoboPlus S/W has been installed automatically, the driver is in LN101 folder of RoboPlus Installation folder.  
    Or if you want to install the newest version, download the newest version VCP driver from FTDI Driver Download page.
    Download Windows 32bit Driver
    Download Windows 64bit Driver


     
  3. Click the Next(N) button to start the installation. Installation of USB Serial Converter driver is completed.

     
  4. Install the USB Serial Port driver in the same way.

 

H/W Specification