LED Module LM-10

Part Photo

[ Picture : LED Module ]

 

Product Usage

The module makes light with LED.  There are two types of LED: Orange and Blue.  ON/OFF of each LED can be controlled separately through port control.

 

 

Pin Assignment Information

  1. OUT2 : The second LED can be turned on when LOW signal is applied.
  2. GND
  3. NC : Not used
  4. VCC
  5. OUT1 : The first LED can be turned on when LOW signal is applied.

Cables can may be damaged when not properly connected (i.e. wrong orientation), or use of excessive force during connection.

 

 

H/W Specification

 

Controller can be installed

 

RoboPlus Task Supports

 

Videos

OLLO Troubleshooting