ROBOTIS e-Manual v1.08.01

[USB2Dynamixel]
USB2Dynamixel is a device used to operate Dynamixel directly from PC. USB2Dynamixel is connected to USB port of PC, and 3P and 4P connectors are installed so that various Dynamixels can be conntected.
Also, USB2Dynamixel can be used to change from USB port to Serial port on the PC without serial port such as notebook computer, etc. The function is very useful in the cases when the Dynamixel exclusive controllers such as CM-2, CM-2+, CM-5, and CM-510 are connected to USB Port, or when ZIG2Serial is connected to USB port to control robots wirelessly.





| Name | Description |
| Status Display LED | Display power supply, TXD(data writing), and RXD(data reading) status. |
| Function Selection Switch | Select the communication method of TTL, RS-485, and RS-232. |
| 3P Connector | Connect Dynamixels of AX Series through TTL communication. |
| 4P Connector | Connect Dynamixels of DX, RX Series through RS-485 communication. |
| Serial Connector | Change from USB port to Serial port through RS-232 communication. |
The communication mode can be selected by chaning the switch of USB2Dynamixel as below.

1. TTL Communication : Dynamixels using 3-pin port such as AX Series, AX-S1 etc.
2. RS485 Communication : Dynamixels using 4-pin port such as DX Series, RX Series, EX Series etc.
3. RS232 Communication : Controllers using serial cable such as CM-5, CM-510 etc.
The following pictures show the usage of connector pins used by USB2Dynamixel. If you want to use each pin for your own purpose, please use them after you learn the usage of each pin.
[ PIN Figure of 4P / 3P Cable Connctors ]

[ PIN Figure of Serial Connector ]

USB2Dynamixel does not supply power to Dynamixel. Therefore, the power must be supplied separately to operate Dynamixel as the following pictures. Please refer to the explanation page of each Dynamixel regarding proper voltages for each Dynamixel mode.
[ Applying Power to the Dynamixel ]
|
Referring to PIN Figure, apply positive (+) voltage to the #2 PIN of the connector, and negative (-) voltage on #1 PIN of the connector. Since the 2 connectors of Dynamixels are equal, power can be applied at any of.) |
[ Applying power between USB2Dynamixel and Dynamixel ]
|
If power cannot be applied as above, apply the power between USB2Dynamixel and Dynamixel as below.
Separate the power cable on the #2 PIN of USB2Dynamixel connector, and then apply positive(+) voltage. Connect additionally Y-cable to the power cable on the #1 PIN of USB2Dynamixel connector, and then apply negative (-) voltage. |
| If you install the RoboPlus, FTDI Driver (USB2Dynamixel,
USB Downloader (LN-101) driver) is installed together automatically.
If you didn't install the RoboPlus yet, or if the driver is not installed appropriately, please install it manually according to following procedures. |