IR Sensor

Part Photo

ir.jpg

[IR Sensor]

 

Product Usage

 

Pin Layout Information

ir_pin.png

  1. SIG1 : Maintains low signal
  2. GND
  3. ADC : Outputs the value detected from IR receiver into analog signals
  4. VCC ( 3.3V )
  5. SIG2 : Can turn on the LED by sending High Signals

Cables can may be damaged when not properly connected (i.e. wrong orientation), or use of excessive force during connection.

 

Make connections to the controlled while unpowered.

Making connections while the controller is powered may cause it to malfunction or/and damage.  

 

Relation between distance and sensor value

ir_graph.png

  

H/W Specification

 

 

Compatible Controllers

 

RoboPlus Task Supports

 

Videos

OLLO Troubleshooting