Robots for Intermediate Level

The following robots have joints less than 8.

The robots can be built with 4 additional AX-12+ to Beginner Kit or Comprehensive Kit.

Please refer to the assembly manual for Bioloid Comprehensive Kit.

 

 

  1. Probing Robot
    probingrobot.jpg

    - Check Assembly

    btn_download.gif  BIO_CMP_ProbingRobot_Check _EN.tsk

    - Task code for Demo

    btn_download.gif  BIO_CMP_ProbingRobot_EN.tsk

    - How to Operate

    • Operate the Probing Robot after installing a various size of obstacles on driving path.
    • Please check if it drives avoiding too big obstacles.
    • Please checks if it lifts up and puts down small obstacles aside to keep driving.  

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4] : Wheel Mode

    • AX-12+ ID[5], ID[6], ID[7] : Joint Mode

    • AX-S1 ID[100]

     
  2. Excavator
    excavator.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_Excavator_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_Excavator_EN.tsk

    - How to Operate

    • Operate the excavator after installing obstacles on the driving path.
    • Please check if it rotates into the detected direction and excavates with robot arms when obstacles are detected from a sensor.

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4] : Wheel Mode

    • AX-12+ ID[5], ID[6], ID[7], ID[8] : Joint Mode

    • AX-S1 ID[100]

     
  3. Robot Flower

    flower.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_RobotFlower_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_RobotFlower_EN.tsk

    - Motion File for Demo

    btn_download.gif BIO_CMP_RobotFlower_EN.mtn

    - How to Operate

    • In bright place, it will blossom out and move slowly as if it is dancing.

    • In dark place, it will close up its petals into a bud.

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4], ID[5], ID[6] : Joint Mode

    • AX-S1 ID[100]

     
  4. Fawn
    fawn.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_Fawn_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_Fawn_EN.tsk

    - Motion File for Demo

    btn_download.gif BIO_CMP_Fawn_EN.mtn

    - How to Operate

    • The Fawn will sit down and look around, when there are no changes.  
    • If you put on an object ahead of its face, it will keep following the objects.

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4], ID[5], ID[6], ID[7] : Joint Mode

    • AX-S1 ID[100]

     
  5. Turtle
    turtle.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_Turtle_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_Turtle_EN.tsk

    - Motion File for Demo

    btn_download.gif BIO_CMP_Turtle_EN.mtn

    - How to Operate

    • Operate the turtle after installing obstacles on the walking path

    • Please check if the turtle avoids the obstacles during its moving.  

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4], ID[5], ID[6], ID[7], ID[8] : Joint Mode

    • AX-S1 ID[100]

     
  6. Spider
    spider.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_Spider_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_Spider_EN.tsk

    - Motion File for Demo

    btn_download.gif BIO_CMP_Spider_EN.mtn

    - How to Operate

    • It will attack if it detects an object ahead of its head during walking.

    • It will pretend to being dead, if it detects an object upper of its head during walking.

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4], ID[5], ID[6], ID[7], ID[8] : Joint Mode

    • AX-S1 ID[100]

     
  7. GerWalk
    gerwalk.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_GerWalk_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_GerWalk_EN.tsk

    - Motion File for Demo

    btn_download.gif BIO_CMP_GerWalk_EN.mtn

    - How to Operate

    • Place an obstacle in the gerwalk’s path then turn on.
    • Detects and avoids obstacles while walking.

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4], ID[5], ID[6], ID[7] : Joint Mode

    • AX-S1 ID[100]

     
  8. Battle Droid
    battledroid.jpg

    - Check Assembly

    btn_download.gif BIO_CMP_BattleDroid_Check _EN.tsk

    - Task Code for Demo

    btn_download.gif BIO_CMP_BattleDroid_EN.tsk

    - Motion File for Demo

    btn_download.gif BIO_CMP_BattleDroid_EN.mtn

    - How to Operate

    • Operate the battle droid after installing obstacles on the walking path.
    • It will attack obstacles with its both arms during its walking.  
    • When the battle droid is fallen down, it will stand up by itself, if you clap out for more than 3 times.

    play.jpg     See Vdieo

    - Dynamixel Setting

    • AX-12+ ID[1], ID[2], ID[3], ID[4], ID[5], ID[6], ID[7], ID[8] : Joint Mode

    • AX-S1 ID[100]