Advanced Level Example Robot (Bioloid Premium)

 Each assembly manuals are downloadable when there is internet connection.

 

 

  1. Dinosour

    Robot Picture

    Category

    Description

    prm_dinosaur.jpg - Level Advanced
    - Algorithm Object detection and motion control using IR Sensor value.
    - Operation Guide
    • Place an obstacle in the robots path and turn the dinosaur robot on.
    • The dinosaur robot attacks.

    • When the obstacle disappears, it continues walking.

    • When nothing is detected for a while, it will sleep.

    - Used Device

    CM-510(1), AX-12+(15), IR Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Lable, Jump, If, Else If, Else, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[15] : Joint Mode

    play.jpg     See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Dinosaur_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Dinosaur_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Dinosaur_EN.mtn
     
  2. Puppy

    Robot Picture

    Category

    Description

    prm_puppy.jpg - Level Advanced
    - Algorithm Motion control depending on the sound detection of the IR Sensor and Timer.
    - Operation Guide
    • Place an obstacle in the robots path and turn the puppy robot on.
    • When a sound is detected, it will walk avoiding obstacles.

    • If you touch its mouth, it will do cute things.
      (It will do different things depending on the number of claps.)

    • When nothing is detected for a while, it will sleep.

    - Used Device

    CM-510(1)(Sound Detection, Timer), AX-12+(17), IR Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Lable, Jump, If, Else If, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[17] : Joint Mode

    play.jpg    See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Puppy_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Puppy_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Puppy_EN.mtn
     
  3. King Spider

    Robot Picture

    Category

    Description

    prm_kingspider.jpg - Level Advanced
    - Algorithm Application motion control depending on the sound detection of the IR Sensor and Timer.
    - Operation Guide
    • When it detects an object while walking, it will avoid it.
    • It will attack when something is detected near the front.

    • When an object is detected above it, it will crumple up its body.

    • When nothing is detected for a while, it will sleep.

    - Used Device

    CM-510(1)(Timer), AX-12+(18), IR Sensor(2)

    - RoboPlus Language

    Function, Call, Load, Lable, Jump, If, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[18] : Joint Mode

    play.jpg     See Video

    - Assembly Manual btn_download.gif  BIO_PRM_KingSpider_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Kingspider_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Kingspider_EN.mtn
     
  4. Scorpion

    Robot Picture

    Category

    Description

    prm_scorpion.jpg - Level Advanced
    - Algorithm Application motion control depending on the number of sounds detected and DMS Sensor value.
    - Operation Guide
    • The robot sleeps when you first turn it on.
    • The robot will awake when you clap.

    • If you clap twice when the robot is awake, it will run away.

    • The closer your hand gets to the sensor, the tail will rise to threaten you.

    • If you get too close, it will attack..

    - Used Device

    CM-510(1)(Sound detection), AX-12+(18), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Lable, Jump, If, Else If, Loop For, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[18] : Joint Mode

    play.jpg     See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Scorpion_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Scorpion_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Scorpion_EN.mtn
     
  5. Lizard

    Robot Picture

    Category

    Description

    prm_lizard.jpg - Level Advanced
    - Algorithm Obstacle avoidance motion control using the IR Sensor and DMS Sensor value.
    - Operation Guide
    • It will being crawling once turned on, and will stop when it detects an object then avoid it.
    • When the tail is caught, it will try to escape.

    - Used Device

    CM-510(1), AX-12+(14), IR Sensor(1),DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Calculate, Endless Loop, If, Else If, Else, Wait  While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[14] : Joint Mode

    play.jpg     See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Lizard_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Lizard_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Lizard_EN.mtn