Use the CM-510's buttons to set the mode and use the buttons and sensor value to control the rotation direction.
- Operation Guide
Press the U button together with the START button on the CM-510 to change to CONTROL mode.
Press the D button together with the START button on the CM-510 to change to FREE mode.
When you press the L button in CONTROL mode, it moves forward. The R button moves backward, U button moves rights, and the D button moves left. A melody will play each time it moves.
When front sensor detects an object in FREE mode, it will turn right. When the lower sensor detects something, it will avoid the edge and turn right.