Intermediate Level Example Robots (Bioloid Premium)

 Each assembly manuals are downloadable when there is internet connection.

 

 

  1. Probing Robot

    Robot Picture

    Category

    Description

    prm_provingrobot.jpg - Level Intermediate
    - Algorithm

    Object sensing and processing depending on IR Sensor's and DMS Sensor's value

    - Operation Guide
    • Place objects of various sizes in the robot's path, then turn the robot on.
    • If the obstacle is too big, it will avoid it.

    • If the obstacle is not too big, it will move it then proceed going its way.

    - Used Device

    CM-510(1), AX-12+(7),IR Sensor(1), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Return, Load, Calculate, Endless Loop, If, Else, Wait While, Break Loop

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[4] : Wheel Mode
    • AX-12+ ID[5]~ ID[7] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_ProbingRobot_ASM_eng.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Probingrobot_EN.tsk
     
  2. Excavator

    Robot Picture

    Category

    Description

    prm_excavator.jpg - Level Intermediate
    - Algorithm Dynamixel Position control depending on IR Sensor's and DMS Sensor's value.
    - Operation Guide
    • Place an object in the robot's path, then turn the robot on.
    • When an object is detected in front of it, it will begin excavating.

    • If an object is detected while carrying an object, the robot will turn in that direction and put the object it was carrying down.

    - Used Device

    CM-510(1), AX-12+(8), IR Sensor(1), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Calculate, Endless Loop, If, Else, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[4] : Wheel Mode
    • AX-12+ ID[5]~ ID[8] : Joint Mode

    play.jpg     See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Excavator_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Excavator_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_RPM_Excavator_EN.mtn
     
  3. Robot Flower

    Robot Picture

    Category

    Description

    prm_robotflower.jpg - Level Intermediate
    - Algorithm Motion control depending on the number of time sound is detected.
    - Operation Guide
    • When the power is turned on, the flower blooms and moves as though it is dancing.
    • If one clap is detected, the petals will pucker up slowly.

    • If several claps are detected, the petals will pucker up quickly.

    - Used Device

    CM-510(1)(Sound Detection), AX-12+(6)

    - RoboPlus Language

    Function, Call, Load,Endless Loop, If, Else, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[6] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_RobotFlower_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Robotflower_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_RobotFlower_EN.mtn
     
  4. Fawn

    Robot Picture

    Category

    Description

    prm_fawn.jpg - Level Intermediate
    - Algorithm Object sensing using IR Sensor's value.
    - Operation Guide
    • When no change is detected, the fawn sits down and looks around.
    • If an object is detected in front of the face, the fawn will follow the object.

    - Used Device

    CM-510(1)(Sound Detection), AX-12+(7), IR Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Endless Loop, If, Else If, Else, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[7] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Fawn_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Fawn_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Fawn_EN.mtn
     
  5. Turtle

    Robot Picture

    Category

    Description

    prm_tuttle.jpg - Level Intermediate
    - Algorithm Avoids obstacles depending on the IR Sensor and DMS Sensor value.
    - Operation Guide
    • Place an obstacle in the robots path and turn the robot on.
    • The turtle avoids obstacles in front of it.

    - Used Device

    CM-510(1), AX-12+(8), IR Sensor(2), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Endless Loop, If, Else If, Else, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[8] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_Turtle_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Turtle_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_Turtle_EN.mtn
     
  6. GerWalk

    Robot Picture

    Category

    Description

    prm_gerwalk.jpg - Level Intermediate
    - Algorithm Control the Bird's walking pattern using the IR Sensor and DMS Sensor value.
    - Operation Guide
    • Place an obstacle in the robots path and turn the gerwalk robot on.
    • The robot avoids obstacles in front of it and on the sides.

    - Used Device

    CM-510(1), AX-12+(7), IR Sensor(2), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Endless Loop, If, Else If, Else, Loop While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[7] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_GerWalk_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_GerWalk_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_GerWalk_EN.mtn
     
  7. Battle Droid

    Robot Picture

    Category

    Description

    prm_battledroid.jpg - Level Intermediate
    - Algorithm Dynamixel control using the IR Sensor's value
    - Operation Guide
    • Place an obstacle in the robots path and turn the battle droid robot on.
    • When the robot detects an object while walking, it will attack with both arms.

    • When battle droid falls down, it will know which side it has fallen up and get up on its own.

    - Used Device

    CM-510(1), AX-12+(8), IR Sensor(1)

    - RoboPlus Language

    Variables, Function, Call, Load, Calculate, Endless Loop, If, Else If, Else, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[8] : Joint Mode

    play.jpg     See Video

    - Assembly Manual btn_download.gif  BIO_PRM_BattleDroid_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_BattleDroid_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_BattleDroid_EN.mtn
     
  8. Quadruped Robot

    Robot Picture

    Category

    Description

    prm_quadrupedwalkingrobot.jpg - Level Intermediate
    - Algorithm Control the walking using the IR Sensor and DMS Sensor value
    - Operation Guide
    • Place an obstacle in the robots path and turn the quadruped robot on.
    • The robot avoids obstacles in front of it.

    - Used Device

    CM-510(1), AX-12+(8), IR Sensor(1), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Endless Loop, If, Wait While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[8] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_QuadrupedRobot_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_QuadrupedRobot_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_QuadrupedRobot_EN.mtn
     
  9. Biped Walking Machine

    Robot Picture

    Category

    Description

    prm_bipedwalkingrobot.jpg - Level Intermediate
    - Algorithm Control the walking using the IR Sensor and DMS Sensor value
    - Operation Guide
    • Place an obstacle in the robots path and turn the robot on.
    • The robot avoids obstacles in front of it and on the sides.

    - Used Device

    CM-510(1), AX-12+(8), IR Sensor(1), DMS Sensor(1)

    - RoboPlus Language

    Function, Call, Load, Endless Loop, If, Else If, Else, Wait While, Loop While

    - Dynamixel Setting
    • AX-12+ ID[11]~ ID[18] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_BipedRobot_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_BipedRobot_EN.tsk
    - MTN File for Demo. btn_download.gif  BIO_PRM_BipedWalkingRobot_EN.mtn
     
  10. Robot Arm

    Robot Picture

    Category

    Description

    prm_robotarm.jpg - Level Intermediate
    - Algorithm Dynamixel Communication for Position Value
    - Operation Guide
    • •Check whether the responding motor reacts to the control motor's movement.
    - Used Device

    CM-510(1), AX-12+(8)

    - RoboPlus Language

    Function, Call, Load, Calculate, Endless Loop, If, Else, Loop While

    - Dynamixel Setting
    • AX-12+ ID[1]~ ID[8] : Joint Mode

    play.jpg      See Video

    - Assembly Manual btn_download.gif  BIO_PRM_RobotArm_ASM_EN.pdf
    - TSK Code for Demo. btn_download.gif  BIO_PRM_Robotarm_EN.tsk