ROBOTIS DREAM SET A Examples

For more information assembly and operation, please refer to the ROBOTIS DREAM SET B workbook.

The controller initially comes with the comprehensive program pre-installed in it.

To create your own program or download, click here to read more on how to “Download the task code.”

You will need the USB cable to download the programs. This is included in ROBOTIS DREAM SET A.

 

  1. Example program of each chapter 4

Explorer

E-1

  1.  Windmill

  "Not Programmable"  

  2.  Avoider

    DREAM_L2_Avoider_EN.tsk

  3.  Scorpion

    DREAM_L2_Scorpion_EN.tsk

  4. Crocodile

    DREAM_L2_Crocodile_EN.tsk