ROBOTIS DREAM SET B Examples

For more information assembly and operation, please refer to the ROBOTIS DREAM SET B workbook.

The controller initially comes with the comprehensive program pre-installed in it.

To create your own program or download, click here to read more on how to “Download the task code.”

You will need the USB cable to download the programs. This is included in ROBOTIS DREAM SET A.

 

  1. Example program of each chapter 4

Explorer

E-1

  1. Probing Car

    DREAM_L3_ Probing Car_EN.tsk

  2. Electric Guitar

    DREAM_L3_Electric Guitar_EN.tsk

  3. Flag Game Robot

    DREAM_L3_Flag Game Robot_EN.tsk

  4. War Robot

    DREAM_L4_War Robot_EN.tsk