ROBOTIS e-Manual v1.13.01

[MX-64T] [MX-64R]
※ Control Table’s Compliance replaced by PID.
※ The control table’s order for PID has changed to DIP from this version onwards. Please make reference of this change.
※ Although the MX-28T (TTL) and MX-28R (RS-485) differ in communications protocols both have the same features and perform equally. (TTL uses 3-pin connectors while RS-485 uses 4)
POSITION SENSOR : Contactless absolute encoder (12BIT,360 DEGREE)
MOTOR : Maxon
BAUD RATE : 8000 bps ~ 4.5 Mbps
CONTROL ALGORITHM : PID CONTROL
Resolution : 0.088°
Gear Reduction Ratio : 200 : 1
6.0N.m (at 12V, 4.1A)
7.3N.m (at 14.8V, 5.2A)
58rpm (at 11.1V)
63rpm (at 12V)
78rpm (at 14.8V)
MX-64T (Half duplex Asynchronous Serial Communication (8bit,1stop, No Parity))
MX-64R (RS485 Asynchronous Serial Communication (8bit,1stop, No Parity))
MX-64T (TTL Level Multi Drop Bus)
MX-64R (RS485 Multi Drop Bus)
Precautions when connecting to power supply! - For the stable power supply, we recommend using ROBOTIS controller or SMPS2Dynamixel. - Connect your DYNAMIXEL to power supply while it’s off and turn on/off with the power switch. |
Control Table consists of data regarding the current status and operation, which exists inside of Dynamixel. The user can control Dynamixel by changing data of Control Table via Instruction Packet.
EEPROM and RAM
Data in RAM area is reset to the initial value whenever the power is turned on while data in EEPROM area is kept once the value is set even if the power is turned off.
Address
It represents the location of data. To read from or write data to Control Table, the user should assign the correct address in the Instruction Packet.
Access
Dynamixel has two kinds of data: Read-only data, which is mainly used for sensing, and Read-and-Write data, which is used for driving.
Initial Value
In case of data in the EEPROM Area, the initial values on the right side of the below Control Table are the factory default settings. In case of data in the RAM Area, the initial values on the right side of the above Control Tables are the ones when the power is turned on.
Highest/Lowest Byte
In the Control table, some data share the same name, but they are attached with (L) or (H) at the end of each name to distinguish the address. This data requires 16bit, but it is divided into 8bit each for the addresses (low) and (high). These two addresses should be written with one Instruction Packet at the same time.
Area |
Address (Hexadecimal) |
Name |
Description |
Access |
Initial Value (Hexadecimal) |
E E P R O M |
0 (0X00) |
Lowest byte of model number |
R |
54 (0X36) |
|
1 (0X01) |
Highest byte of model number |
R |
1 (0X01) |
||
2 (0X02) |
Information on the version of firmware |
R |
- |
||
3 (0X03) |
ID of Dynamixel |
RW |
1 (0X01) |
||
4 (0X04) |
Baud Rate of Dynamixel |
RW |
34 (0X22) |
||
5 (0X05) |
Return Delay Time |
RW |
250 (0XFA) |
||
6 (0X06) |
Lowest byte of clockwise Angle Limit |
RW |
0 (0X00) |
||
7 (0X07) |
Highest byte of clockwise Angle Limit |
RW |
0 (0X00) |
||
8 (0X08) |
Lowest byte of counterclockwise Angle Limit |
RW |
255 (0XFF) |
||
9 (0X09) |
Highest byte of counterclockwise Angle Limit |
RW |
15 (0X0F) |
||
11 (0X0B) |
Internal Limit Temperature |
RW |
80 (0X50) |
||
12 (0X0C) |
Lowest Limit Voltage |
RW |
60 (0X3C) |
||
13 (0X0D) |
Highest Limit Voltage |
RW |
160 (0XA0) |
||
14 (0X0E) |
Lowest byte of Max. Torque |
RW |
255 (0XFF) |
||
15 (0X0F) |
Highest byte of Max. Torque |
RW |
3 (0X03) |
||
16 (0X10) |
Status Return Level |
RW |
2 (0X02) |
||
17 (0X11) |
LED for Alarm |
RW |
36 (0X24) |
||
18 (0X12) |
Shutdown for Alarm |
RW |
36 (0X24) |
||
R A M |
24 (0X18) |
Torque On/Off |
RW |
0 (0X00) |
|
25 (0X19) |
LED On/Off |
RW |
0 (0X00) |
||
26 (0X1A) |
Derivative Gain |
RW |
0 (0X00) |
||
27 (0X1B) |
Integral Gain |
RW |
0 (0X00) |
||
28 (0X1C) |
Proportional Gain |
RW |
32 (0X20) |
||
30 (0X1E) |
Lowest byte of Goal Position |
RW |
- |
||
31 (0X1F) |
Highest byte of Goal Position |
RW |
- |
||
32 (0X20) |
Lowest byte of Moving Speed |
RW |
- |
||
33 (0X21) |
Highest byte of Moving Speed |
RW |
- |
||
34 (0X22) |
Lowest byte of Torque Limit |
RW |
ADD14 |
||
35 (0X23) |
Highest byte of Torque Limit |
RW |
ADD15 |
||
36 (0X24) |
Lowest byte of Current Position |
R |
- |
||
37 (0X25) |
Highest byte of Current Position |
R |
- |
||
38 (0X26) |
Lowest byte of Current Speed |
R |
- |
||
39 (0X27) |
Highest byte of Current Speed |
R |
- |
||
40 (0X28) |
Lowest byte of Current Load |
R |
- |
||
41 (0X29) |
Highest byte of Current Load |
R |
- |
||
42 (0X2A) |
Current Voltage |
R |
- |
||
43 (0X2B) |
Current Temperature |
R |
- |
||
44 (0X2C) |
Means if Instruction is registered |
R |
0 (0X00) |
||
46 (0X2E) |
Means if there is any movement |
R |
0 (0X00) |
||
47 (0X2F) |
Locking EEPROM |
RW |
0 (0X00) |
||
48 (0X30) |
Lowest byte of Punch |
RW |
0 (0X00) |
||
49 (0X31) |
Highest byte of Punch |
RW |
0 (0X00) |
||
68 (0X44) |
Lowest byte of Consuming Current |
RW |
0 (0X00) |
||
69 (0X45) |
Highest byte of Consuming Current |
RW |
0 (0X00) |
||
70 (0X46) |
Torque control mode on/off |
RW |
0 (0X00) |
||
71 (0X47) |
Lowest byte of goal torque value |
RW |
0 (0X00) |
||
72 (0X48) |
Highest byte of goal torque value |
RW |
0 (0X00) |
||
73 (0X49) |
Goal Acceleration |
RW |
0 (0X00) |
It represents the Model Number.
It represents the firmware version.
It is a unique number to identify Dynamixel.
The range from 0 to 253 (0xFD) can be used,
and, especially, 254(0xFE) is used as the Broadcast ID.
If the Broadcast ID is used to transmit Instruction Packet, we can command
to all Dynamixels.
| Please be careful not to duplicate the ID of connected Dynamixel. |
It is the baud rate to communicate with controller. It is available in between 0~254(0XFE).
If the data value is in between 0~249 :
Baudrate(BPS) = 2000000 / (Data + 1)
Data |
Set BPS |
Target BPS |
Tolerance |
1 |
1000000.0 |
1000000.0 |
0.000 % |
3 |
500000.0 |
500000.0 |
0.000 % |
4 |
400000.0 |
400000.0 |
0.000 % |
7 |
250000.0 |
250000.0 |
0.000 % |
9 |
200000.0 |
200000.0 |
0.000 % |
16 |
117647.1 |
115200.0 |
-2.124 % |
34 |
57142.9 |
57600.0 |
0.794 % |
103 |
19230.8 |
19200.0 |
-0.160 % |
207 |
9615.4 |
9600.0 |
-0.160 % |
If the date value is over the 250 :
Data |
Set BPS |
Target BPS |
Tolerance |
250 |
2250000.0 |
2250000.0 |
0.000 % |
251 |
2500000.0 |
2500000.0 |
0.000 % |
252 |
3000000.0 |
3000000.0 |
0.000 % |
Note : Maximum Baud Rate error of 3% is within the tolerance of UART communication. |
It is the delay time per data value that takes from the transmission of Instruction Packet until the return of Status Packet.
0 to 254 (0xFE) can be used, and the delay time per data value is 2 usec.
That is to say, if the data value is 10, 20 usec is delayed. The initial value is 250 (0xFA) (i.e., 0.5 msec).
The angle limit allows the motion to be restrained.
The range and the unit of the value is the same as Goal Position(Address
30, 31).
The following two modes can be set pursuant to the value of CW and CCW.
Operation Type |
CW / CCW |
Wheel Mode |
the value of the both are 0 |
Joint Mode |
the value of the both are not 0 |
The wheel mode can be used to wheel-type operation robots since motors of the robots spin infinitely.
The joint mode can be used to multi-joints robot since the robots can be controlled with specific angles.
It is the highest limit of operating temperature.
The range for use is 10 to 99 (0x10~0x63). The unit is Celsius.
For example, if the value is 80, it is 80℃.
If the internal temperature of Dynamixel exceeds this range, Over Heating Error Bit (Bit2) of Status Packet is returned as ‘1’ and Alarm is triggered as set in the addresses 17 and 18.
Caution : Do not set the temperature lower/higher than the default value. When the temperature alarm shutdown occurs, wait 20 minutes to cool the temperature before re-use. Using the product when the temperature is high may and can cause damage. |
The Lowest (Highest) Limit Voltage
It is the operation range of voltage.
50 to 250 (0x32 ~ 0x96) can be used. The unit is 0.1V.
For example, if the value is 80, it is 8V.
If Present Voltage (Address42) is out of the range, Voltage Range Error Bit (Bit0) of Status Packet is returned as ‘1’ and Alarm is triggered as set in the addresses 17 and 18.
It is the torque value of maximum output. 0 to 1023 (0x3FF) can be used, and the unit is about 0.1%.
For example, Data 1023 (0x3FF) means that Dynamixel will use 100% of the maximum torque it can produce while Data 512 (0x200) means that Dynamixel will use 50% of the maximum torque. When the power is turned on, Torque Limit (Addresses 34 and 35) uses the value as the initial value.
It decides how to return Status Packet. There are three ways like the below table.
Value |
Return of Status Packet |
0 |
No return against all commands (Except PING Command) |
1 |
Return only for the READ command |
2 |
Return for all commands |
When Instruction Packet is Broadcast ID, Status Packet is not returned regardless of Status Return Level. |
Dynamixel can protect itself by detecting errors occur during the operation.
The errors can be set are as the table below.
Bit |
Name |
Contents |
Bit 7 |
0 |
- |
Bit 6 |
Instruction Error | When undefined Instruction is transmitted or the Action command is delivered without the reg_write command |
Bit 5 |
Overload Error | When the current load cannot be controlled with the set maximum torque |
Bit 4 |
CheckSum Error | When the Checksum of the transmitted Instruction Packet is invalid |
Bit 3 |
Range Error | When the command is given beyond the range of usage |
Bit 2 |
OverHeating Error | When the internal temperature is out of the range of operating temperature set in the Control Table |
Bit 1 |
Angle Limit Error | When Goal Position is written with the value that is not between CW Angle Limit and CCW Angle Limit |
Bit 0 |
Input Voltage Error | When the applied voltage is out of the range of operating voltage set in the Control Table |
It is possible to make duplicate set since the function of each bit is run by the logic of ‘OR’. That is, if 0X05 (binary 00000101) is set, both Input Voltage Error and Overheating Error can be detected.
If errors occur, in case of Alarm LED, the LED blinks; in case of Alarm Shutdown, the motor output becomes 0 % by making the value of Torque Limit(Address 34, 35) as 0.
Value |
Meaning |
0 |
Keeps Torque from generating by interrupting the power of motor. |
1 |
Generates Torque by impressing the power to the motor. |
Value |
Meaning |
0 |
Turn OFF the LED. |
1 |
Turn ON the LED. |
MX series will use the PID controller as a main control method.
P gain refers to the value of proportional band.
I gain refers to the value of integral action.
D Gain refers to the value of derivative action.
Gains values are in between 0~254.


※ The relationship between Compliance Slop and PID
The less the P gain, The larger the back lash, and the weaker the amount of output near goal position. At some extent, it is like a combined concept of margine and slope. It does not exactly match the previous concept of compliance. So it is obvious if you see the difference in terms of motion. ※ Explanation for PID required. For the brief explanation about general PID, please refer to the website(link) below. http://en.wikipedia.org/wiki/PID_controller FYI, PID control theory is not only limited to the control of motor(actuator) but is a generic theory that can be applied to all kinds of control. |
It is a position value of destination.
0 to 7095 (0xFFF) is available. The unit is 0.088 degree.
If Goal Position is out of the range, Angle Limit Error Bit (Bit1) of Status Packet is returned as ‘1’ and Alarm is triggered as set in Alarm LED/Shutdown.

Join Mode
It is a moving speed to Goal Position.
0~1023 (0X3FF) can be used, and the unit is about 0.114rpm.
If it is set to 0, it means the maximum rpm of the motor is used without
controlling the speed.
If it is 1023, it is about 117.07rpm.
For example, if it is set to 300, it is about 34.33 rpm.
Wheel Mode
It is a moving speed to Goal direction.
0~2047 (0X7FF) can be used, and the unit is about 0.114rpm.
If a value in the range of 0~1023 is used, it is stopped by setting
to 0 while rotating to CCW direction.
If a value in the range of 1024~2047 is used, it is stopped by setting
to 1024 while rotating to CW direction.
That is, the 10th bit becomes the direction bit to control the direction.
Notes: Please check the maximum rpm of relevant model. Even if the motor is set to more than maximum rpm, it cannot generate the torque more than the maximum rpm. |
It is the value of the maximum torque limit.
0 to 1023 (0x3FF) is available, and the unit is about 0.1%.
For example, if the value is 512, it is about 50%; that means only 50%
of the maximum torque will be used.
If the power is turned on, the value of Max Torque (Address 14, 15) is
used as the initial value.
Notes: If the function of Alarm Shutdown is triggered, the motor loses its torque because the value becomes 0. At this moment, if the value is changed to the value other than 0, the motor can be used again. |
It is the current position value of Dynamixel.
The range of the value is 0~4095 (0xFFF), and the unit is 0.088 degree.

Is the current moving speed.
0~2047 (0x000~0X7FF) can be used.
If a value is in the rage of 0~1023 then the motor rotates to the CCW direction.
If a value is in the rage of 1024~2047 then the motor rotates to the CW direction.
The 10th bit becomes the direction bit to control the direction; 0 and 1024 are equal.
The value unit is about 0.11rpm.
For example, if it is set to 300 then the motor is moving to the CCW direction at a rate of about 34.33rpm.
It means currently applied load.
The range of the value is 0~2047, and the unit is about 0.1%.
If the value is 0~1023, it means the load works to the CCW direction.
If the value is 1024~2047, it means the load works to the CW direction.
That is, the 10th bit becomes the direction bit to control the direction, and 1024 is equal to 0.
For example, the value is 512, it means the load is detected in the direction of CCW about 50% of the maximum torque.

Notes: Current load is inferred from the internal torque value, not from Torque sensor etc. For that reason, it cannot be used to measure weight or torque; however, it must be used only to detect which direction the force works. |
It is the size of the current voltage supplied.
This value is 10 times larger than the actual voltage. For example, when 10V is supplied, the data value is 100 (0x64)
It is the internal temperature of Dynamixel in Celsius.
Data value is identical to the actual temperature in Celsius. For example, if the data value is 85 (0x55), the current internal temperature is 85℃.
Value |
Meaning |
0 |
There are no commands transmitted by REG_WRITE |
1 |
There are commands transmitted by REG_WRITE. |
| Notes: If ACTION command is executed, the value is changed into 0. |
Value |
Meaning |
0 |
Goal position command execution is completed. |
1 |
Goal position command execution is in progress. |
Value |
Meaning |
0 |
EEPROM area can be modified. |
1 |
EEPROM area cannot be modified. |
| Caution: If Lock is set to 1, the power must be turned off and then turned on again to change into 0. |
Current to drive motor is at minimum.
Can choose vales from 0x00 to 0x3FF.
Value at 2048(0x800) when current is consumption is idle.
Values higher than 2048(0x800) during positive current flow
Values lower than 2048(0x800) during negative current flow
The following is a method to calculate current flow
I = ( 4.5mA ) * (CURRENT – 2048 ) in amps unit (A).
For example, 68 gives a value of 2148, which corresponds to 450mA of current flow.

Value |
Meaning |
0 |
Turn off the torque mode. Executes Joint mode or Wheel mode. |
1 |
Turn on the torque mode. Cannot control the position or moving speed but only Torque. |
When Torque Control Mode Enable is at 1, DYNAMIXEL behaves like the followings
1. DYNAMIXEL does not control the position or the moving speed.
2. DYNAMIXEL controls with goal torque value.
3. DYNAMIXEL does not react to whatever value in Goal position and Goal speed.
4. Because position/moving speed is not controller, DYNAMIXEL behaves as if it is in the wheel mode.
These are the goal torque value
You can use 0 ~ 2047 (0x7FF), and the unit is 4.5mA.
(torque is directly proportional to the current value.)
If you use from 0~1023, torque is on toward CCW, and when you set it to 0, it stops.
If you use from 1024~2047, torque is on toward CW, and when you set it to 1024, it stops.
That means, 10th bit becomes the direction bit, which controls direction.
Goal Torque cannot be bigger than Torque Limit(34,35)
This is Goal Acceleration value.
It can be used from 0~254(0XFE), and the unit is approximately 8.583 Degree / sec^2.
When it is set to 0, there is no control over acceleration and moves with the maximum acceleration of the motor.
When the goal speead is set to 0, there is no control over acceleration and moves with the maximum acceleration of the motor.
When it is set to 254, it becomes 2180 Degree / sec^2
For example, the current speed of Dynamixel is 0, and Goal acceleration is 10,
The speed of Dynamixel after 1 second will be 14.3 RPM.
The types of MX-64 option frame are as follows.




The types of MX-64 Horn are as follows.


Ref: place careful attention when aligning the horn of the RX-64 to prevent misalignment. |
The following example shows the combination structure of option frames and horns.

Drawing Information :
RX64Dimension.pdf
HOW TO REPLACE GEARS