ROBOTIS e-Manual v1.09.00
Dynamixel SDK for Windows can be downloaded.
[System Requirements]
▶ OS : Windows XP/Vista/7 (32/64bit)
▶ USB2Dynamixel is required.
▶ In case DLL loading is not available : Needs to install Microsoft Visual C++ 2005 re-distribution package.
| If you install the RoboPlus, FTDI Driver (USB2Dynamixel,
USB Downloader (LN-101) driver) is installed together automatically.
If you didn't install the RoboPlus yet, or if the driver is not installed appropriately, please install it manually according to following procedures. |





The response speed must be reset to make the response speed of USB2Dynamixel and Dynamixel faster.
How to set the response speed is as follows.
1. If you go to Control Panel - System - Device Manager, you can find USB Serial Port as below.

2. Click "Advanced" button from "Select Port" tab of registration information window.

3. Set the Response Time Adjustment in BM-related setting to 1 as the picture below, and click "Confirm" button.

The folder structure of Dynamixel SDK for Windows is as follows:
/bin : DLL files for Windows are included.
/import : necessary files for programming are included.
/src : DLL sources are included.
/example : Examples to control Dynamixel for users' programming environment are included.
If you want to execute a program developed by Dynamixel SDK, dynamixel.dll is requred.
dynamixel.dll is included in bin folder of Dynamixel SDK.
If you register the location of dynamixel.dll as an environment variable for Windows, dll is not necessary when the program is executed.
If you do not want to register the location of dll as environment variables, the program and dll must be distributed together.
1. If you go to Control Panel - System - Advanced, you can find Environment Variable as below.

2. Find Path category in system variables, and then click "Edit" button.

3. Add bin folder to the end of existing variable values with semicolon under the example folder.
Please be careful not to change or delete the existing variable values.
The example below shows added things, assuming the location of DLL file is C:\Project\bin.

Please refer to the following links for examples pursuant to programming environment.