Dynamixel SDK
Dynamixel SDK is a standard programming library to develop S/W controls Dynamixel.
The characteristics of Dynamixel SDK are as below:
- It has outstading portability in each platform since written in C language.
- It is easy to peform platform porting since it is written both platform independent and dependent sources.
- The interface is standardized; thus, the developed software can be used again even if the controller is different.