Boot Loader

Boot Loader makes the users possible to use the controller.  Boot Loader cannot be erased by the users.  If it is broken down, the controller cannot be used.  Boot Loader is built-in on the controller when it is manufactured in the factory.

 

 

The available commands in Boot Loader can be found using "Help" command.

bootloaderhelp.png