ROBOTIS e-Manual v1.14.00
The program start position can be set by APP/SYS command. Once the program start position is set, the program is executed on the program start position when the power is turned on or reset.
The memory map using Atmega2561 is as below.

(Most programs such as provided firmware, user program etc. start from 0 address, if there are no specific reasons.)
(It is started as Boot Loader status, even if you do not press "#.")