ROBOTIS e-Manual v1.13.01
AVR Studio provides users various Macro, Library, and comprehensive environment for easy programming.
AVR Studio can be downloaded from the website below, and it is free-of-charge.
http://www.atmel.com/dyn/products/tools_card.asp?tool_id=2725
The installation procedure is as follows.
1. The initial wildow is as below.

2. The window below is about license agreement. You must agree to continue the installation.

3. Select a folder for the installation, and then click "Next" button.

4. The window below is about a driver installation regarding ISP. If there are no specific reasons, install the driver.

5. Click "Next" to continue the installation.

6. Start AVR Studio installation.

7. AVR Studio installation is completed.