Installing WinAVR
WinAVR is necessary for AVR programming.
WinAVR can be downloaded from the following website, and it is free-of-charge.
http://winavr.sourceforge.net/
The installation process is as below.
1. Select a language.
2. The initial window is as below.
3. The window below is about the license agreement. You must agree to continue the installation.
4. Select a folder for the installation, and then click "Next" button.
5. Select programs and environment options. If there are no specific reasons, it is recommended to install all in the list.
6. Start WinAVR installation.
7. WinAVR installation is completed.