ROBOTIS e-Manual v1.13.01
Verify successful installation.by opening a sample project.
Decompress the file (no root user rights needed).

When you first run Eclipse, it requires to set up workspace like the picture below.

* if you leave the default path, it may not be able to read the project. Please change it to another path.
Click on the left lower box to prevent this window.
Run Eclipse and go to File – New – Makefile Project with Existing Code.

Click on Browse select 01 LED and click on Verify.

After selecting the project go to Project – Clean, Build

To see progress check the terminal window
If progress is not as shown below then check the working development environment.