ROBOTIS e-Manual v1.09.00
It makes the users possible to develop their own firmware.
The characteristics are as follows:
If you want to use Embedded C, you need the knowledge of software and hardware. If you are a beginner, we recommend you use Embedded C after learing the software and the hardware. If you use Embedded C, you cannot use RoboPlus since the controller's firmware is changed. If you want to use RoboPlus again, you must restore the firmware using RoboPlus. |
Currently the following controllers are supported:.