ROBOTIS e-Manual v1.08.01
These commands will branch the flow of the program depending on whether the condition is true or false.
Else If: Execute if the clause is true and previous clause ("if" or "else if" clause) is false. This is the equivalent of the "else if" statement in C language.
Else: Execute if none of the conditions are true. This is the equivalent of the "else" statement in C language.
Conditional clause is a feature to perform different actions depending on whether the condition evaluates to true (condition is met) or false (condition is not met).
Conditional clause is composed of the following 3 parts: parameter 1, relational operator, and parameter 2 in order.
![]()
These are 6 types of relational operators.

!= : True if the two parameters are not equal.
>= : True if parameter 1 is greater than or equal to parameter 2.
> : True if parameter 1 is greater than parameter 2.
<= : True parameter 1 is less than or equal to parameter 2.
< : True if parameter 1 is less than parameter 2.
Conditional clause can be combined into a complex conditional clause using conditional operators.
A complex conditional clause is composed of the following 3 parts: conditional clause 1, conditional operator, conditional clause 2.
![]()
There are 3 types of conditional operators.

then : Does not link any clauses.
AND(&&): True if both conditional clauses are true.
OR(||): True if one of the conditional clauses is true.
There is no limit to how many conditional clauses can be combined into one complex conditional clause. Each conditional clause is evaluated in order, and the final value will be either "true" or "false."
A block, designated by brackets, needs to follow each clause.
(However, if the block consists of only one line, the block
need not be enclosed with brackets.)

o When the variable is greater than or equal to 90.
o When the variable is greater than or equal to 50 and less than 90.
o Other cases