Endless Loop Last
updated 2010.1.18 (v1.0 Eng)
This command is used to repeat the command lines in the block without
end.
Usage
- A block is always required. (However, if the block consists of
only one, the block need not be enclosed with brackets.)

- Use the "Break Loop"
command to exit the loop.
Example