Loop While

This command is used to repeat the command lines in the block while the clause is true.

It is the equivalent of the "while"function in C language..

 

What is a conditional clause?

Conditional clause is a feature to perform different actions depending on whether the condition evaluates to true (condition is met) or false (condition is not met).  

Conditional clause is composed of the following 3 parts: parameter 1,  relational operator, and parameter 2 in order.   

program_condition_1.png

These are 6 types of  relational operators.

program_condition_2.png

Conditional clause can be combined into a complex conditional clause using conditional operators.  

A complex conditional clause is composed of the following 3 parts: conditional clause 1, conditional operator, conditional clause 2.

program_condition_3.png

There are 3 types of conditional operators.

program_condition_4.png

There is no limit to how many conditional clauses can be combined into one complex conditional clause.  Each conditional clause is evaluated in order, and the final value will be either "true" or "false."

 

Usage

 

Example

program_while_condition_2.png