Button Count
This parameter is used to read how many times the START button was pressed when the controller was first turned on.
Compatible Controller
Characteristic
- "Button Counts" uses numbers between 0 and 255. As a result, only up to 255 button presses can be counted .
Example
- The example executes different motions according to how many times the START button was pressed - once, twice, or more.