ROBOTIS e-Manual v1.13.01
This parameter is used to transmit data via a wireless communication module (IR, zigbee module).
When the "Remocon TXD" parameter is set, the data is immediately sent wirelessly.
In the example below, the program waits for data, and when the data arrives, the received data is transmitted wirelessly.

This parameter is used to read the received data received via the wireless communication module (IR, zigbee module).
The "Remocon Arrived" parameter can be used check for new data.
You can save up to maximum 2 wireless data by using a receiving buffer.
When 2 data are saved in the receiving buffer, firstly received data will be read at first, and the remaining data will be read at second according to the received order. If there is only 1 data value in the buffer, when READ is executed, the latest data will be retrieved.

This parameter is used to check whether there are any new data received via the wireless communication module(IR, zigbee module).
![]() |
|
|