ROBOTIS e-Manual v1.13.01
These parameters are used to set or read the actuator's margin value.
![]()
These parameters are used to set or read the actuator's slope value.
The slope value will be created at both CW/CCW directions, and the output level will be set near the target position.
If you set the lower slope value, it will reach to the target position by reducing the initial power NOT that much. On the contrary, if you set the higher value, it will reach the target position by reducing considerable powers as it reaches to the goal.
If you set the lower slope value, it will resist with maximum power not to stray from target position.
Even if you set the higher value, it will resist with more and more power if it is strayed too much from target position.
Compliance Slope will be changed into 7 Data representative values according to the input Data. In other words, if you input 25, in real operation, 16 -the representative value of 25-, will be used.
Level |
Real Data Value |
Representative Data Value |
1 |
0 (0x00) ~ 3(0x03) |
2 (0x02) |
2 |
4(0x04) ~ 7(0x07) |
4 (0x04) |
3 |
8(0x08)~15(0x0F) |
8 (0x08) |
4 |
16(0x10)~31(0x1F) |
16 (0x10) |
5 |
32(0x20)~63(0x3F) |
32 (0x20) |
6 |
64(0x40)~127(0x7F) |
64 (0x40) |
7 |
128(0x80)~254(0xFE) |
128 (0x80) |
Appropriate Compliance Slope, Power control, and the Compliance Margin values will make it possible to create smoother movement.
![]()