Print Program Output
Controllers usually do not have display devices the way a PC has
a monitor, so it is hard to keep track of what goes on in a controller.
Therefore, a "terminal" is used to "borrow"
the PC's monitor.

RoboPlus Task includes a terminal program to display the status of the
controller.
Open the Program Output Monitor
To see the output of the program, you must open the Program
Output Monitor BEFORE executing the
program.
There are three ways to open the Program Output Monitor.
- Click the 'View Print of Program'
on the Download Program window.

- Click the "View Print of
Program" button in the tool
bar.
- Press F5 or
Click on "View
Print of Program (V)" menu under Program
(P).
Print / Print with carriage return

- Print : Print the value, then move the cursor to next line.

- Print with New Line: Print out the value, and move the cursor to
next line.

Error : Please check the following
- Values from the controller
- Values from task code
All decimal numbers between -32767 and +32767 can be displayed. (Printing
characters or custom messages is not possible.)
- To print numbers

- To print values from sensors

Clear Screen
- You may erase everything on the screen.