ROBOTIS e-Manual v1.08.01
※ Download : ROBOTIS Website Database ( Open Link in New Window )
RoboPlus is a software to create a customized programme for every ROBOTIS product.

<RoboPlus System Requirements>
▶ OS : Windows XP SP2 more / Vista / 7 (32/64bit)
▶ 32-Bit (x86) or 64 Bit (x64) Processor over 800MHz
▶ Graphic card with 3D acceleration function
▶ System memory over 512MB
▶ Hard disk with the extra space of 500MB

| Notes
: To execute RoboPlus, .NET FrameWork 3.5 or higher version is
required.
When installing RoboPlus, if the automatic installation of .NET FrameWork fails, .NET FrameWork must be installed separately. |
When RoboPlus installation is finished, the following icon is appeared on the screen.

Executing RoboPlus, you can also execute the included programs.

RoboPlus includes following programs.