ROBOTIS OpenCM IDE

The ROBOTIS OpenCM is a development Software and download tool for the OpenCM9.04 embedded board.

Sources of the ROBOTIS OpenCM are released under licenses of their respective authors

Copyright (c)  ROBOTIS Co., Ltd. Modified or newly-created codes are released under the GNUGPL or LGPL licenses.

For more information on the OpenCM9.04 refer to the Appendix section of the e-manuals

 

GNU GPL

GNL LGPL

OpenCM9.04 Software Download

OpenCM9.04 uses the ROBOTIS OpenCM Integrated Developmental Environment (IDE) to allow users to program with ease. The download link for the ROBOTIS OpenCM IDE can be found below:

[Windows XP, Vista, 7, 8] 32bit/64bit

ROBOTIS-v1.0.4-windows.zip

 

[Mac OS X] Tested in OS X 10.12.2

ROBOTIS_OpenCM-v1.0.3-macosx.zip

 

[Linux 64bit] Tested in Ubuntu 12.04

ROBOTIS_OpenCM-v1.0.2-linux64.tgz

 

[Linux 32bit] Tested in Ubuntu 10.10

ROBOTIS_OpenCM-v1.0.2-linux32.tgz

 

Getting started