Zigbee SDK
Zigbee SDK is a standard programming library to develop S/W communicates with RoboPlus Task with RoboPlus Task code.
The characteristics of Zigbee SDK are as below.
- It has outstanding portability in each platform since written in C language.
- It is easy to perform platform porting since it is written in both platform independent and dependent sources.
- The interface is standardized; thus, the developed software can be used again even if the controller is different.